Represents the cone surface geometry to provide access to information about the faces of a solid.
Remarks
The Cone object is one of several surface geometrical elements that can be used to return information from the faces of a solid. Faces of a solid can be extracted using the Faces and FacesByRay properties on the model and feature objects where each face is returned as a topological object. The geometric information is obtained from the face by using the Geometry property of the topological object.