| Class Module | Description |
|---|---|
| Body | Provides a set of interfaces that allow you to access the topological and sense data that is related to the object. |
| BSplineCurve | Describes the 3-D B-Spline curve. |
| BSplineSurface | Describes the B-Spline surface of the faces of a solid. |
| Circle | Represents the circle surface geometry to provide access to information about the faces of a solid. |
| Cone | Represents the cone surface geometry to provide access to information about the faces of a solid. |
| Curve | Represents an occurrence of a curve topological entity. |
| CurveBody | Represents an instance of a construction surface. |
| CurvePath | Represents an occurrence of a collection of curves presented in sequential order. |
| CurvePaths | Represents a collection of CurvePath objects. |
| Curves | Represents a collection of Curve objects. |
| CurveVertex | Holds the topological position of the endpoint of an Edge. |
| CurveVertices | Represents a collection of Vertices. |
| Cylinder | Represents the cylinder surface geometry to provide access to information about the faces of a solid. |
| Edge | Represents the elemental piece of the 3-D geometry information for the boundaries of a Face. |
| Edges | Represents a collection of Edges. |
| EdgeUse | Represents the use of a given Edge in a loop. |
| EdgeUses | Represents a collection of EdgeUses. |
| Ellipse | Represents the ellipse surface geometry to provide access to information about the faces of a solid. |
| Face | Represents the elemental piece of surface data that makes up the body. |
| Faces | Represents a collection of Faces. |
| Line | Describes a Line in 3-D space. |
| Loop | Represents a closed contour on a given Face. |
| Loops | Represents a collection of Loops. |
| ParamBSplineCurve | Describes the 2-D B-Spline curve. |
| Plane | Represents the plane surface geometry to provide access to information about the faces of a solid. |
| Shell | Represents a set of connected Faces. |
| Shells | Represents a collection of Shells. |
| Sphere | Represents the sphere surface geometry to provide access to information about the faces of a solid. |
| Torus | Represents the torus surface geometry to provide access to information about the faces of a solid. |
| Vertex | Holds the topological position of the endpoint of an Edge. |
| Vertices | Represents a collection of Vertices. |
| Enumeration | Description |
|---|---|
| FeatureTopologyQueryTypeConstants | Feature Topology Query Type Constants |
| GNTTypePropertyConstants | GNT Type Property Constants |
| SmartCollectionTypeConstants | Smart Collection Type Constants |
| TopologyCollectionTypeConstants | Topology Collection Type Constants |