Solid Edge Geometry Type Library
CurveBody Object
Members 
Description
Represents an instance of a construction surface.
Object Model
CurveBody ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionCurvePaths CollectionCurves CollectionCurveVertices Collection
Remarks
A CurveBody is represented by the Curves and the CurvePaths that define the shape of the surface.
See Also

CurveBody Members

Send comments on this topic.