Solid Edge Geometry Type Library
IsParamReversed Property
Collapse All
Expand All
Solid Edge Geometry Type Library
>
Curve Object
: IsParamReversed Property
Description
Returns a Boolean value to specify whether or not the inherent direction of the referenced object is opposed to the flow dicated by the parameterization of the underlying geometry.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsParamReversed As Boolean
See Also
Curve Object
|
Curve Members
Send comments
on this topic.