Solid Edge Geometry Type Library
Cylinder Object
Members 
Description
Represents the cylinder surface geometry to provide access to information about the faces of a solid.
Remarks
Faces of a solid can be extracted using the Faces and FacesByRay methods on the model and feature objects where each face is returned as a topological object. The geometric information is obtained from the face by using the Geometry property of the topological object.
See Also

Cylinder Members

Send comments on this topic.