Application | Returns the active application object. |
Edge | Returns the Edge object for the referenced EdgeUse object. |
Geometry | Returns a 3-D geometry object whose properties and methods can extend to the topology collection. |
IsClosed | Returns a Boolean value to specify whether or not the start and end points of the referenced object are coincident. |
IsOpposedToEdge | Specifies whether or not the referenced EdgeUse object is opposed to another edge or not. |
IsParamReversed | Returns a Boolean value to specify whether or not the inherent direction of the referenced object is opposed to the flow dicated by the parameterization of the underlying geometry. |
Loop | Represents a closed contour on a given Face. |
Next | Returns the next EdgeUse object. |
Parent | Returns the parent object for the referenced object. |
Partner | Returns the partner EdgeUse ojbect. |
Previous | Returns the previous EdgeUse object. |
Type | Returns a member of the GNTTypePropertyConstants set to indicate the type of the referenced object. |