Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objBody As SolidEdgeGeometry.Body
Dim objEdge As SolidEdgeGeometry.Edge
Dim lngContinuity As Long
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' creating the base feature
If CreateModel(objDoc) <> "" Then
MsgBox "Error creating the model"
Exit Sub
End If
' getting the body object of the model
Set objBody = objDoc.Models(1).Body
'getting an edge from the edges collection of the body object
Set objEdge = objBody.Edges(EdgeType:=igQueryAll).Item(1)
' getting the continuity value for an edge
lngContinuity = objEdge.Continuity
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objBody = Nothing
Set objEdge = Nothing
End Sub