Solid Edge Geometry Type Library
Add Method
Specifies the Edge, Face, or Vertex to be added to the collection.
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Sub Add( _
   ByVal Item As Object _
) 
Parameters
Item
Specifies the Edge, Face, or Vertex to be added to the collection.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBody As solidedgegeometry.Body
    Dim objFaces As Object
    Dim objFacesCol As Object
    Const TESTFILE = "T:\vbtests\testcases\freeform.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    ' Close active document if any
    Call objDoc.Close
    ' Open a testcase file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Get the body object of the model
    Set objBody = objDoc.Models(1).Body
    'Create an userdefined faceCollection object
    Set objFacesCol = objBody.CreateCollection(Type:=seFaceCollection)
    'Get the Faces of the body object
    Set objFaces = objBody.Faces(FaceType:=igQueryAll)
    ' Add few items to faceCollection
    Call objFacesCol.Add(objFaces(1))
    Call objFacesCol.Add(objFaces(3))
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objFaces = Nothing
    Set objFacesCol = Nothing
End Sub
See Also

Faces Collection  | Faces Members

Send comments on this topic.