Solid Edge Geometry Type Library
IsUserDefined Property
Description
Specifies whether or not the referenced collection has had edges or faces manually added to it.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsUserDefined As Boolean
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBody As solidedgegeometry.Body
    Dim objFacesCol As Object
    Const TESTFILE = "T:\vbtests\testcases\freeform.par"
    Dim bIsUserDefined As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    ' Close active document if any
    Call objDoc.Close
    ' Open a testcase file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Get the body object of the model
    Set objBody = objDoc.Models(1).Body
    'Create an userdefined FacesCollection object
    Set objFacesCol = objBody.CreateCollection(Type:=seEdgeCollection)
    'Capture the FacesCollection status
    bIsUserDefined = objFacesCol.IsUserDefined
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objFacesCol = Nothing
End Sub
See Also

Faces Collection  | Faces Members

Send comments on this topic.