Solid Edge Geometry Type Library
RemoveAll Method
Description
Removes all objects from the referenced object.
Syntax
Visual Basic
Public Sub RemoveAll() 
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBody As solidedgegeometry.Body
    Dim objFaces As Object
    Dim objFacesCol As Object
    Const TESTFILE = "T:\vbtests\testcases\freeform.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    ' Close active document if any
    Call objDoc.Close
    ' Open a testcase file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Get the body object of the model
    Set objBody = objDoc.Models(1).Body
    'Create an userdefined faceCollection object
    Set objFacesCol = objBody.CreateCollection(Type:=seFaceCollection)
    ' Get the Faces of the body object
    Set objFaces = objBody.Faces(FaceType:=igQueryAll)
    ' Add few Faces to the collection
    Call objFacesCol.Add(objFaces(1))
    Call objFacesCol.Add(objFaces(4))
    Call objFacesCol.Add(objFaces(2))
    'RemoveAll items from the FacesCollection object
    Call objFacesCol.RemoveAll
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objFaces = Nothing
    Set objFacesCol = Nothing
End Sub
See Also

Faces Collection  | Faces Members

Send comments on this topic.