Solid Edge Geometry Type Library
FacetCount Property
Description
Returns the number of facets on the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property FacetCount( _
   ByVal Tolerance As Double _
) As Long
Parameters
Tolerance
Example
Private Sub Form_Load()
    Dim objApp As solidedgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBody As solidedgegeometry.Body
    Dim objFace As solidedgegeometry.Face
    Dim lngFacetCount As Long
    Const TESTFILE = "T:\vbtests\testcases\FreeForm.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    Call objDoc.Close
    ' opening the testfile
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting the body object of the model
    Set objBody = objDoc.Models(1).Body
    ' getting a particular face from the collection of faces on the body
    Set objFace = objBody.Faces(FaceType:=igQueryAll).Item(4)
    ' getting the FacetCount for a Face
    lngFacetCount = objFace.FacetCount(TOLERANCE:=0.01)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objFace = Nothing
End Sub
See Also

Face Object  | Face Members

Send comments on this topic.