Solid Edge Geometry Type Library
GetNormal Method
Specifies the number of points to be evaluated.
Returns the array of parametric points at which to evaluate the surface normals.
Returns the array of unit-vectors normal to the surface.
Description
Given an array of parametric points, returns normal unit vectors.
Syntax
Visual Basic
Public Sub GetNormal( _
   ByVal NumParams As Long, _
   ByRef Params() As Double, _
   ByRef Normals() As Double _
) 
Parameters
NumParams
Specifies the number of points to be evaluated.
Params
Returns the array of parametric points at which to evaluate the surface normals.
Normals
Returns the array of unit-vectors normal to the surface.
Example
Private Sub Form_Load()
    Dim objApp As solidedgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBody As solidedgegeometry.Body
    Dim objFace As solidedgegeometry.Face
    Dim dblParam(3) As Double
    Dim dblNormal() As Double
    Const TESTFILE = "T:\vbtests\testcases\HalfCyl.par"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening the testfile
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting the body object of the model
    Set objBody = objDoc.Models(1).Body
    ' getting a particular face from the collection of faces on the body
    Set objFace = objBody.Faces(FaceType:=igQueryAll).Item(2)
    ' getting the normal at a point (u=0.5, v=0.5) on a Face
    dblParam(0) = 3 * PI / 2
    dblParam(1) = 0.1
    dblParam(2) = PI / 2
    dblParam(3) = 0.05
    Call objFace.GetNormal(NumParams:=2, Params:=dblParam, Normals:=dblNormal)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objFace = Nothing
End Sub
See Also

Face Object  | Face Members

Send comments on this topic.