Application | Returns the active application object. |
Body | Returns the Body of the Loop. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
EdgeUses | Returns a collection of EdgeUse objects for the referenced Loop. |
Face | Returns the Face object for the referenced Loop object. |
ID | Returns the Parasolid ID of the Loop. |
IsOuterLoop | Returns True if the referenced object is an outer loop. |
Parent | Returns the parent object for the referenced object. |
Tag | Returns the Tag of the Loop. |
Type | Returns a member of the GNTTypePropertyConstants set to indicate the type of the referenced object. |
Vertices | Returns the vertices that are bounded by the current Loop. |