Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objPBCurve As solidedgegeometry.ParamBSplineCurve
    Dim lngNumKnots As Long
    Const TESTFILE = "T:\vbtests\testcases\freeform.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening the test case file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting a ParamBSplineCurve from the test case
    Set objPBCurve = objDoc.Models(1).Body.Shells(1).Faces(1).Loops(1).EdgeUses(1).Geometry
    ' getting the number of knots
    lngNumKnots = objPBCurve.GetNumKnots
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPBCurve = Nothing
End Sub