Solid Edge Geometry Type Library
GetNormalVector Method
Returns a unit vector that is perpendicular to the referenced plane.
Description
Returns a unit vector that is perpendicular to the referenced plane.
Syntax
Visual Basic
Public Sub GetNormalVector( _
   ByRef NormalVector() As Double _
) 
Parameters
NormalVector
Returns a unit vector that is perpendicular to the referenced plane.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objModel As SolidEdgePart.Model
    Dim ObjFace As solidedgegeometry.Face
    Dim objPlane As Object
    Dim dblNVector() As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create base feature
    If CreateModel(objDoc) <> "" Then
        MsgBox "Error creating the model"
        Exit Sub
    End If
    'Get a handle to Model
    Set objModel = objDoc.Models(1)
    'Get the BottomCap of the protrusion
    Set ObjFace = objModel.ExtrudedProtrusions(1).BottomCap
    'Get the Plane object from Face
    Set objPlane = ObjFace.Geometry
    Call objPlane.GetNormalVector(NormalVector:=dblNVector)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objModel = Nothing
    Set ObjFace = Nothing
    Set objPlane = Nothing
End Sub
See Also

Plane Object  | Plane Members

Send comments on this topic.