Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objModel As SolidEdgePart.Model
    Dim ObjFace As solidedgegeometry.Face
    Dim objPlane As Object
    Dim dblRPoint() As Double
    Dim dblReqRelAccy As Double
    Dim dblArea As Double
    Dim dblMoments() As Double
    Dim dblPrincipalAxes() As Double
    Dim dblRelAccyAchieved As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create base feature
    If CreateModel(objDoc) <> "" Then
        MsgBox "Error creating the model"
        Exit Sub
    End If
    'Get a handle to Model
    Set objModel = objDoc.Models(1)
    'Get the BottomCap of the Protrusion
    Set ObjFace = objModel.ExtrudedProtrusions(1).BottomCap
    'Get the Plane object
    Set objPlane = ObjFace.Geometry
    dblReqRelAccy = 0.0001
    Call objPlane.GetPlaneProperties(ReqRelAccy:=dblReqRelAccy, Area:=dblArea, RootPoint:=dblRPoint(), _
                                     Moments:=dblMoments, PrincipalAxes:=dblPrincipalAxes, RelAccyAchieved:=dblRelAccyAchieved)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objModel = Nothing
    Set ObjFace = Nothing
    Set objPlane = Nothing
End Sub