Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objModel As SolidEdgePart.Model
Dim ObjFace As solidedgegeometry.Face
Dim objPlane As Object
Dim dblRPoint() As Double
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Create base feature
If CreateModel(objDoc) <> "" Then
MsgBox "Error creating the model"
Exit Sub
End If
'Get a handle to Model
Set objModel = objDoc.Models(1)
'Get the BottomCap of the Protrusion
Set ObjFace = objModel.ExtrudedProtrusions(1).BottomCap
'Get the Plane object
Set objPlane = ObjFace.Geometry
Call objPlane.GetRootPoint(RootPoint:=dblRPoint)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objModel = Nothing
Set ObjFace = Nothing
Set objPlane = Nothing
End Sub