Solid Edge Geometry Type Library
Volume Property
Collapse All
Expand All
Solid Edge Geometry Type Library
>
Shell Object
: Volume Property
Description
Indicates the volume of the referenced object in cubic meters.
Property type
Read-only property
Syntax
Visual Basic
Public Property Volume As Double
Remarks
This property is successful only when the Body or Shell is a solid (that is, it encloses a finite volume).
See Also
Shell Object
|
Shell Members
Send comments
on this topic.