| Solid Edge Geometry Type Library : Torus Object | 
|  GetAxisVector | Returns the unit vector that defines the axis of the referenced object. | 
|  GetCenterPoint | Returns the point that is the center of the referenced object. | 
|  GetTorusData | Returns the surface geometry data on the referenced Torus object. | 
|  Application | Returns the active application object. | 
|  MajorRadius | Returns or sets the radius of the major axis for the referenced object. | 
|  MinorRadius | Returns or sets the radius of the minor axis for the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Type | Returns a member of the GNTTypePropertyConstants set to indicate the type of the referenced object. |