Solid Edge Geometry Type Library
Add Method
Specifies the Edge, Face, or Vertex to be added to the collection.
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Sub Add( _
   ByVal Item As Object _
) 
Parameters
Item
Specifies the Edge, Face, or Vertex to be added to the collection.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBody As solidedgegeometry.Body
    Dim objFaces As Object
    Dim objVertices As Object
    Dim objVertexCollection As Object
    Const TESTFILE = "T:\vbtests\testcases\freeform.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    ' Close active document if any
    Call objDoc.Close
    ' Open a testcase file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Get the body object of the model
    Set objBody = objDoc.Models(1).Body
    'Create an userdefined VertexCollection object
    Set objVertexCollection = objBody.CreateCollection(Type:=seVertexCollection)
    ' Get the Faces on the Body
    Set objFaces = objBody.Faces(FaceType:=igQueryAll)
    'Get the Vertices collection object
    Set objVertices = objFaces(1).Vertices
    ' Add few vertices to the Collection
    Call objVertexCollection.Add(objVertices(1))
    Call objVertexCollection.Add(objVertices(3))
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objFaces = Nothing
    Set objVertices = Nothing
    Set objVertexCollection = Nothing
End Sub
See Also

Vertices Collection  | Vertices Members

Send comments on this topic.