Solid Edge Geometry Type Library
Count Property
Description
Returns the number of objects in the referenced collection.
Property type
Read-only property
Syntax
Visual Basic
Public Property Count As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objVertices As Object
    Dim objBody As solidedgegeometry.Body
    Dim objFaces As Object
    Const TESTFILE = "T:\vbtests\testcases\Vertices.par"
    Dim lngCnt As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Open the TestFile
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Get the Body object
    Set objBody = objDoc.Models(1).Body
    ' Get the Faces on the Body
    Set objFaces = objBody.Faces(FaceType:=igQueryAll)
    ' Get the Vertices collection object
    Set objVertices = objFaces(1).Vertices
    'Get the Count property of Vertices object
    lngCnt = objVertices.Count
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objVertices = Nothing
    Set objBody = Nothing
    Set objFaces = Nothing
End Sub
See Also

Vertices Collection  | Vertices Members

Send comments on this topic.