Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BendAngle | Sets and returns the angle of the bend with respect to the stationary portion of the face to which the bend is added. |
BendDirection | Sets and returns a constant that specifies the direction in which the MovingSide will move to create the new face. |
BendParamType | Sets and returns the method to be used when specifying the bend neutral factor. |
BendPZLSide | Sets and returns a constant value that specifies the location of the created bend and face with respect to the profile. |
BendRadius | Sets and returns the inside radius of the bend. |
BendReliefDepth | Sets and returns the depth of the bend relief for the specified object. |
BendReliefType | Sets and returns a constant that specifies the Bend relief type. |
BendReliefWidth | Sets and returns the width of the bend relief. |
BendState | Sets and returns a constant that specifies whether the feature is created in the bent state or the flattened state. |
CornerReliefType | Sets and returns the corner relief type. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
ExtendBendRelief | |
ExtendMoldLines | Sets and returns a constant that specifies whether or not to extend mold lines. |
ExtentSide | Sets and returns the reference plane side for the referenced object. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
MovingSide | Sets and returns a constant that specifies the side of the base part, with respect to the profile, that will move to become the created face. |
Name | Returns the name of the referenced object. |
NeutralFactor | Sets and returns the neutral factor applied to the bend. |
Parent | Returns the parent object for the referenced object. |
Profile | Sets and returns the Profile object used to construct the referenced feature object. |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |
UseGlobalBendRadius | Specifies whether or not the global bend radius is to be applied to the referenced object. |
UseGlobalBendReliefDepth | Specifies whether or not the global bend relief depth is to be applied to the referenced object. |
UseGlobalBendReliefWidth | Specifies whether or not the global bend relief width is to be applied to the referenced object. |
UseGlobalNeutralFactor | Specifies whether or not the global neutral factor is to be applied to the referenced object. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |