Solid Edge Part Type Library
BendDirection Property
Collapse All
Expand All
Solid Edge Part Type Library
>
Bend Object
: BendDirection Property
Description
Sets and returns a constant that specifies the direction in which the MovingSide will move to create the new face.
Property type
Read-write property
Syntax
Visual Basic
Public Property BendDirection As
BendFeatureConstants
Remarks
The BendDirection is indicated as either along or opposite the profile plane normal (that is, as either a convex or a concave bend). Valid values are members of the BendFeatureConstants constant set.
See Also
Bend Object
|
Bend Members
Send comments
on this topic.