|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  ClosureType | Sets and returns the closer type for the referenced CloseCorner object. | 
|  CornerGap | Sets or returns the face gap distance of the referenced CloseCorner object. | 
|  CutAngle | Sets or returns the angle of the referenced CloseCorner with V-Shaped treatment. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. | 
|  Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. | 
|  FacesByRay | Returns a collection of faces that are intersected by a specified vector. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  OffsetValue | Sets or returns the offset value of the referenced CloseCorner cutout. | 
|  OverlapRatio | Sets or returns the overlap ratio of the referenced CloseCorner object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  ShowDimensions | Controls the display of dimensions for the feature object. | 
|  SquareSize | Sets or returns the square size of the referenced CloseCorner with square cutout treatment. | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  SuppressVariable | Returns the suppress variable object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  TreatmentDiameter | Sets or returns the diameter of the circular bend relief of the referenced CloseCorner object. | 
|  TreatmentType | Sets and returns the type of treatment for the referenced object. | 
|  Type | Specifies the type of the object being referenced. | 
|  Visible | Specifies whether or not the referenced object is displayed to the screen. |