Solid Edge Part Type Library
TreatmentDiameter Property
Collapse All
Expand All
Solid Edge Part Type Library
>
CloseCorner Object
: TreatmentDiameter Property
Description
Sets or returns the diameter of the circular bend relief of the referenced CloseCorner object.
Property type
Read-write property
Syntax
Visual Basic
Public Property TreatmentDiameter As Double
Remarks
Requires that the TreatmentType property is seCloseCnrTreatmentCircularCutout.
See Also
CloseCorner Object
|
CloseCorner Members
Send comments
on this topic.