| Solid Edge Part Type Library : CrossBrake Object | 
|  Delete | Deletes the referenced object. | 
|  Reorder | Inserts the referenced object in front of or behind another feature. | 
|  RollToFeature | Rolls the referenced Model object back to a specified feature. | 
|  Application | Returns the active application object. | 
|  BendAngle | |
|  BendDirection | |
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  Faces | |
|  Lines | |
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  SuppressVariable | Returns the suppress variable object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  Type | Specifies the type of the object being referenced. |