Solid Edge Part Type Library
Faces Property
Description
Property type
Read-write property
Syntax
Visual Basic
Public Property Faces As Object
Remarks
The result of the Faces property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used. By default, the Faces property returns all faces for the object. The topology collection can be restricted to a specified type of face by supplying a value (from the FeatureTopologyQueryTypeConstants constant set) for the FaceType argument for the feature objects only. For example, this property can be set to return all faces that are spheres.
See Also

CrossBrake Object  | CrossBrake Members  | Solid Edge V19 - What's New

Send comments on this topic.