| Solid Edge Part Type Library : FEAConnector Object | 
|  Delete | Delete a particular connector. | 
|  GetBoltConnectionOptions | Create a new bolt connector | 
|  GetBoltHeadDiameter | |
|  GetBottomGeometries | |
|  GetConnectorType | Get type of the connector, glue/linear. | 
|  GetConnectorValue | Get the coefficient of static friction value of a linear connector. | 
|  GetFlip | Get current flip condition of connector. | 
|  GetInitialPenetrationTypeValue | |
|  GetMasterGeometries | Get array of master geometry objects (edges/vertices). | 
|  GetMinSearchDistValue | Get minimum search distance value for a connector. | 
|  GetNutDiameter | |
|  GetOIDDirMaps | |
|  GetPenaltyValue | Get penalty value of a glue connector. | 
|  GetPreStressVal | |
|  GetShaftDiameter | |
|  GetSlaveGeometries | Get Slave geometry objects (edges/vertices). | 
|  GetTopGeometries | |
|  SetBoltConnectionOptions | |
|  SetBoltHeadDiameter | |
|  SetBottomGeometries | |
|  SetConnectorType | Set type of the connector. | 
|  SetConnectorValue | Set the coefficient of static friction value of a linear connector. | 
|  SetFlip | Flip connector direction. | 
|  SetInitialPenetrationTypeValue | |
|  SetMasterGeometries | Set master geometry objects (edges/vertices). | 
|  SetMinSearchDistValue | Set minimum search distance value for a connector. | 
|  SetNutDiameter | |
|  SetPenaltyValue | Set penalty value for a glue connector. | 
|  SetPreStressVal | |
|  SetShaftDiameter | |
|  SetSlaveGeometries | Set slave geometry objects (edges/vertices). | 
|  SetTopGeometries |