Solid Edge Part Type Library
SetConnectorType Method
Description
Set type of the connector.
Syntax
Visual Basic
Public Sub SetConnectorType( _
   ByVal eConnectorType As FEAConnectorTypeEnum_Auto _
) 
Parameters
eConnectorType
ValueDescription
eConnectorTypeBoltConnection_Auto 
eConnectorTypeEdgeConnector_Auto 
eConnectorTypeGlue_Auto 
eConnectorTypeGlueEdgeConnector_Auto 
eConnectorTypeLinear_Auto 
eConnectorTypeNone_Auto 
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
        Dim objStudyOwner As SolidEdgePart.StudyOwner = Nothing
        Dim objStudy As SolidEdgePart.Study = Nothing
        Dim objConnectorOwner As SolidEdgePart.ConnectorOwner = Nothing
        Dim objConnector As SolidEdgePart.FEAConnector = Nothing
        Dim eConnectorType As SolidEdgePart.FEAConnectorTypeEnum_Auto

        Try
            OleMessageFilter.Register()

            ' Connect to Solid Edge
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument

            objStudyOwner = objPartDocument.StudyOwner
            objStudy = objStudyOwner.Item(1)
            objStudy.GetConnectorOwner(objConnectorOwner)
            objConnector = objConnectorOwner.Item(1)

            eConnectorType = SolidEdgePart.FEAConnectorTypeEnum_Auto.eConnectorTypeLinear_Auto

            objConnector.SetConnectorType(eConnectorType)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

FEAConnector Object  | FEAConnector Members  | Solid Edge ST3 - What's New

Send comments on this topic.