|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  DieRadius | Sets and returns radius value for the top of the referenced feature. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  Distance | Sets and returns the constraint distance for the referenced object. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. | 
|  Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. | 
|  FacesByRay | Returns a collection of faces that are intersected by a specified vector. | 
|  FormedRadius | This read-write Double property sets and returns the formed radius value for gusset feature. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  MaterialSide | Sets and returns the direction in which material was added to the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  NumberOfOccurrences | Returns the number of occurrences. | 
|  OccurrenceSpacing | This read-write Double property sets and returns the spacing between gusset occurrences in the sheet metal document. | 
|  Parent | Returns the parent object for the referenced object. | 
|  PatternType | Sets and returns the pattern to apply to the referenced Gusset object. | 
|  Profile | Sets and returns the Profile object used to construct the referenced feature object. | 
|  PunchRadius | Sets and returns the radius value at the bottom of the referenced feature. | 
|  Rounding | This read-write Double property specifies whether or not rounding is applied to a gusset feature. | 
|  Shape | This read-write Double property specifies the shape of the gusset in the sheet metal document. | 
|  ShowDimensions | Controls the display of dimensions for the feature object. | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  SuppressVariable | Returns the suppress variable object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  TaperAngle | Sets and returns the taper angle for the referenced object. | 
|  ThicknessSide | Sets and returns the side of the profile on which the thickness of the feature object was added. | 
|  Type | Specifies the type of the object being referenced. | 
|  Width | Returns the width of the referenced object. |