Solid Edge Part Type Library
PatternType Property
Description
Sets and returns the pattern to apply to the referenced Gusset object.
Property type
Read-write property
Syntax
Visual Basic
Public Property PatternType As GussetConstants
Remarks
Depending on the setting of this property, other properties are enabled or disabled. For example, the FillBackGround property is enabled for PatternType = 1, 2, or 3, but is disabled for PatternType = 0.
See Also

Gusset Object  | Gusset Members  | Solid Edge V19 - What's New

Send comments on this topic.