Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBaseProfile As SolidEdgepart.Profile
    Dim objBaseProfArray(1 To 2) As SolidEdgepart.Profile
    Dim objBase As SolidEdgepart.Model
    Dim objCBoreHoleData As SolidEdgepart.HoleData
    Dim objRP As SolidEdgepart.RefPlane
    Dim objCBoreHoleProfile As SolidEdgepart.Profile
    Dim objCBoreHole As SolidEdgepart.Hole
    Dim dblCBDepth As Double
    Dim lngStatus As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' *** creating the an extruded protrusion base feature
    ' creating a circular profile for the base feature and validating it
    Set objBaseProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
    Call objBaseProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.1)
    lngStatus = objBaseProfile.End(ValidationCriteria:=igProfileClosed)
    If (lngStatus <> 0) Then
        MsgBox "Profile for the base feature is not closed"
    End If
    ' creating the extruded protrusion and validating it
    Set objBaseProfArray(1) = objBaseProfile
    Set objBase = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _
                                                            ProfileArray:=objBaseProfArray, ProfilePlaneSide:=igSymmetric, ExtrusionDistance:=0.05)
    objBaseProfile.Visible = False
    If (objBase.ExtrudedProtrusions(1).Status <> igFeatureOK) Then
        MsgBox "AddFiniteExtrudedProtrusion method of models object fails"
    End If
    ' *** creating a CounterBore Hole using the HoleDataCollection object
    ' creating the hole data for a counter bore hole
    Set objCBoreHoleData = objDoc.HoleDataCollection.Add(HoleType:=igCounterboreHole, _
                                                         HoleDiameter:=0.01, CounterboreDiameter:=0.02, CounterboreDepth:=0.01, BottomAngle:=0)
    ' creating a profile for the counter bore hole and validating it
    Set objRP = objDoc.RefPlanes(1)
    Set objCBoreHoleProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objRP)
    Call objCBoreHoleProfile.Holes2d.Add(xcenter:=0.05, ycenter:=0)
    lngStatus = objCBoreHoleProfile.End(ValidationCriteria:=igProfileClosed)
    If (lngStatus <> 0) Then
        MsgBox "Profile for the regular hole is not closed"
    End If
    ' creating the counter bore hole on the base feature and validating it
    Set objCBoreHole = objBase.Holes.AddFinite(Profile:=objCBoreHoleProfile, _
                                               ProfilePlaneSide:=igLeft, FiniteDepth:=0.03, Data:=objCBoreHoleData)
    If (objCBoreHole.Status <> igFeatureOK) Then
        MsgBox "AddFinite method of the Holes object fails"
    End If
    objCBoreHoleProfile.Visible = False
    ' reading and modifying the counterbore depth of the counter bore hole
    dblCBDepth = objCBoreHoleData.CounterboreDepth
    objCBoreHoleData.CounterboreDepth = dblCBDepth + 0.005
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBaseProfile = Nothing
    Set objBaseProfArray(1) = Nothing
    Set objBase = Nothing
    Set objCBoreHoleData = Nothing
    Set objRP = Nothing
    Set objCBoreHoleProfile = Nothing
    Set objCBoreHole = Nothing
End Sub