|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  BottomAngle | Sets and returns the angle of the bottom of a finite hole. | 
|  CounterboreDepth | Sets and returns the depth of the counterbore for an associated Hole object. | 
|  CounterboreDiameter | Sets and returns the diameter of the counterbore for an associated Hole object. | 
|  CounterboreProfileLocationType | Sets or returns the location of the counterbore profile for an associated Hole object by way of the referenced HoleData object. | 
|  CountersinkAngle | Sets and returns the angle of the countersink for an associated Hole object. | 
|  CountersinkDiameter | Sets and returns the diameter of the countersink for an associated Hole object. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  HoleDiameter | Sets and returns the diameter of an associated Hole object. | 
|  HoleType | Sets and returns the type of hole. | 
|  InsideEffectiveThreadLength | Sets and returns the effective thread length associated with the inner diameter. | 
|  InternalThreadDescription | Sets and returns the description associated with the internal diameter of the tapered thread. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  OutsideEffectiveThreadLength | Sets and returns the effective thread length associated with the outer diameter. | 
|  Parent | Returns the parent object for the referenced object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  Taper | Sets and returns the taper type. | 
|  TaperDimType | Specifies whether the Taper dimension is to be specified from the top or the bottom for the referenced HoleData object. | 
|  TaperLValue | Specifies the value to be applied to the hole Length for the referenced HoleData object. | 
|  TaperMethod | Sets and returns the taper definition through the referenced HoleData object. | 
|  TaperRValue | Specifies the value to be applied to the hole Radius for the referenced HoleData object. | 
|  ThreadDataByDescription | Sets and returns thread data by description. | 
|  ThreadDepth | Sets and returns the depth of a thread. | 
|  ThreadDepthMethod | Sets and returns the method in which a thread is defined. | 
|  ThreadDescription | Sets and returns the description of the thread. | 
|  ThreadExternalDiameter | Sets and returns the external diameter of the thread for an associated Hole object. | 
|  ThreadHeight | Sets and returns the thread height. | 
|  ThreadMinorDiameter | Sets and returns the minor diameter of the thread for an associated Hole object. | 
|  ThreadNominalDiameter | Sets and returns the nominal diameter of the thread for an associated Hole object. | 
|  ThreadSetting | Sets and returns the thread setting type. | 
|  ThreadTaperAngle | Sets and returns the taper for the threads. | 
|  TreatmentType | Sets and returns the type of treatment for the referenced object. | 
|  Units | Sets and returns the units in which the line width is defined. | 
|  VBottomDimType | Specifies where dimensions are calculated for the referenced HoleData object when the TaperMethod is set to igVShaped. |