Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBaseProfile As SolidEdgepart.Profile
    Dim objBaseProfArray(1 To 2) As SolidEdgepart.Profile
    Dim objBase As SolidEdgepart.Model
    Dim objRegHoleData As SolidEdgepart.HoleData
    Dim objRP As SolidEdgepart.RefPlane
    Dim objRegHoleProfile As SolidEdgepart.Profile
    Dim objRegHole As SolidEdgepart.Hole
    Dim objAttributeSets As Object
    Dim lngStatus As Long
    Dim bAttribSetPresent As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' *** creating the an extruded protrusion base feature
    ' creating a circular profile for the base feature and validating it
    Set objBaseProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
    Call objBaseProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.1)
    lngStatus = objBaseProfile.End(ValidationCriteria:=igProfileClosed)
    If (lngStatus <> 0) Then
        MsgBox "Profile for the base feature is not closed"
    End If
    ' creating the extruded protrusion and validating it
    Set objBaseProfArray(1) = objBaseProfile
    Set objBase = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _
                                                            ProfileArray:=objBaseProfArray, ProfilePlaneSide:=igSymmetric, ExtrusionDistance:=0.05)
    objBaseProfile.Visible = False
    If (objBase.ExtrudedProtrusions(1).Status <> igFeatureOK) Then
        MsgBox "AddFiniteExtrudedProtrusion method of models object fails"
    End If
    ' *** creating a Regular Hole using the Holedatacollection object
    ' creating the holedata
    Set objRegHoleData = objDoc.HoleDataCollection.Add(HoleType:=igRegularHole, _
                                                       HoleDiameter:=0.01, BottomAngle:=90)
    ' creating the profile for the hole and validating it
    Set objRP = objDoc.RefPlanes.AddParallelByDistance(parentplane:=objDoc.RefPlanes(1), _
                                                       distance:=0.025, normalside:=igRight)
    Set objRegHoleProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objRP)
    Call objRegHoleProfile.Holes2d.Add(xcenter:=0, ycenter:=0)
    lngStatus = objRegHoleProfile.End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox " profile for the hole is not closed"
    End If
    ' creating the hole
    Set objRegHole = objBase.Holes.AddFinite(Profile:=objRegHoleProfile, _
                                             ProfilePlaneSide:=igLeft, FiniteDepth:=0.02, Data:=objRegHoleData)
    If (objRegHole.Status <> igFeatureOK) Then
        MsgBox "AddFinite method of the Holes object fails"
    End If
    objRegHoleProfile.Visible = False
    ' Get the Attributesets collection object
    Set objAttributeSets = objRegHoleData.AttributeSets
    'Create an attributeset
    objAttributeSets.Add "MyAttribSet"
    'Check for the presence of Attributeset
    bAttribSetPresent = objRegHoleData.IsAttributeSetPresent("MyAttribSet")
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBaseProfile = Nothing
    Set objBaseProfArray(1) = Nothing
    Set objBase = Nothing
    Set objRegHoleData = Nothing
    Set objRP = Nothing
    Set objRegHoleProfile = Nothing
    Set objRegHole = Nothing
    Set objAttributeSets = Nothing
End Sub