Solid Edge Part Type Library
Taper Property
Collapse All
Expand All
Solid Edge Part Type Library
>
HoleData Object
: Taper Property
Description
Sets and returns the taper type.
Property type
Read-write property
Syntax
Visual Basic
Public Property Taper As Double
Remarks
Depending on the value of the TaperMethod property, the taper type can be either the ratio of the taper (the hole diameter divided by the unit depth) or the angle of the taper.
See Also
HoleData Object
|
HoleData Members
Send comments
on this topic.