Solid Edge Part Type Library
ThreadDepth Property
Description
Sets and returns the depth of a thread.
Property type
Read-write property
Syntax
Visual Basic
Public Property ThreadDepth As Double
Remarks
This property value can be the actual thread depth or the number of threads depending on the value of the ThreadDepthMethod property.
See Also

HoleData Object  | HoleData Members

Send comments on this topic.