Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objModel As SolidEdgePart.Model
    Dim objProfile As SolidEdgePart.Profile
    Const TESTFILE = "T:\vbtests\testcases\cube.par"
    Const TOLERANCE = 0.0001
    Dim dblDensity As Double
    Dim dblAccuracyIn As Double
    Dim dblAccuracyOut As Double
    Dim dblVolume As Double
    Dim dblArea As Double
    Dim dblMass As Double
    Dim dblCofGravity() As Double
    Dim dblCofVolume() As Double
    Dim dblGlobalMoments() As Double
    Dim dblPrincipalMoments() As Double
    Dim dblPrincipalAxes() As Double
    Dim dblRadiiOfGyration() As Double
    Dim lngStatus As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Close the part document
    Call objDoc.Close
    ' Open a Testcase
    Set objDoc = objApp.Documents.Open(Filename:=TESTFILE)
    ' Get the model object in the test case
    Set objModel = objDoc.Models(1)
    '************************
    ' CASE 1 : Compute the Physical Properties on base model
    '************************
    ' Compute the physical properties on the model.
    dblDensity = 1
    dblAccuracyIn = 0.0001
    Call objModel.ComputePhysicalProperties( _
         Density:=dblDensity, Accuracy:=dblAccuracyIn, Volume:=dblVolume, _
         Area:=dblArea, Mass:=dblMass, CenterOfGravity:=dblCofGravity, _
         CenterOfVolume:=dblCofVolume, _
         GlobalMomentsOfInteria:=dblGlobalMoments, _
         PrincipalMomentsOfInteria:=dblPrincipalMoments, _
         PrincipalAxes:=dblPrincipalAxes, _
         RadiiOfGyration:=dblRadiiOfGyration, _
         RelativeAccuracyAchieved:=dblAccuracyOut, Status:=lngStatus)
    ' Checking the physical properties of model
    If Abs(dblVolume - 0.001) > TOLERANCE Or Abs(dblArea - 0.06) > TOLERANCE Or _
       Abs(dblMass - 0.001) > TOLERANCE Or Abs(dblAccuracyOut - 0.0001) > TOLERANCE Then
        MsgBox ("ComputePhysicalProperties method of Model object fails")
    End If
    '***********************************
    ' CASE 2 : Compute the Physical Properties on updated model
    '***********************************
    'Compute the the physical properties on the updated model. _
     Since the updated model has been not computed so _
     ComputePhysicalProperties should recompute and then return the _
     physical properties of the updated model.
    objModel.ExtrudedProtrusions(1).Depth = 0.125
    ' Compute the physical properties on the updated model.
    dblDensity = 1
    dblAccuracyIn = 0.0001
    Call objModel.ComputePhysicalProperties( _
         Density:=dblDensity, Accuracy:=dblAccuracyIn, Volume:=dblVolume, _
         Area:=dblArea, Mass:=dblMass, CenterOfGravity:=dblCofGravity, _
         CenterOfVolume:=dblCofVolume, _
         GlobalMomentsOfInteria:=dblGlobalMoments, _
         PrincipalMomentsOfInteria:=dblPrincipalMoments, _
         PrincipalAxes:=dblPrincipalAxes, _
         RadiiOfGyration:=dblRadiiOfGyration, _
         RelativeAccuracyAchieved:=dblAccuracyOut, Status:=lngStatus)
    ' Checking the physical properties of updated model
    If Abs(dblVolume - 0.00125) > TOLERANCE Or Abs(dblArea - 0.07) > TOLERANCE Or _
       Abs(dblMass - 0.00125) > TOLERANCE Or Abs(dblAccuracyOut - 0.0001) > TOLERANCE Then
        MsgBox ("ComputePhysicalProperties method of Model object fails")
    End If
    '***********************************
    ' CASE 3 : Compute the Physical Properties on Failed model
    '***********************************
    ' Create a failed feature and Compute physical properties on Failed model
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(objDoc.RefPlanes(1))
    Call objProfile.Circles2d.AddByCenterRadius(0.015, 0.015, 0.005)
    Call objProfile.End(igProfileClosed)
    Call objModel.ExtrudedProtrusions.AddFinite(objProfile, igLeft, igLeft, 0.015)
    If objModel.ExtrudedProtrusions(2).Status <> igFeatureFailed Then
        MsgBox "Failed to create a sick feature"
    End If
    objProfile.Visible = False
    ' Compute the physical properties on the failed model.
    dblDensity = 1
    dblAccuracyIn = 0.0001
    Call objModel.ComputePhysicalProperties( _
         Density:=dblDensity, Accuracy:=dblAccuracyIn, Volume:=dblVolume, _
         Area:=dblArea, Mass:=dblMass, CenterOfGravity:=dblCofGravity, _
         CenterOfVolume:=dblCofVolume, _
         GlobalMomentsOfInteria:=dblGlobalMoments, _
         PrincipalMomentsOfInteria:=dblPrincipalMoments, _
         PrincipalAxes:=dblPrincipalAxes, _
         RadiiOfGyration:=dblRadiiOfGyration, _
         RelativeAccuracyAchieved:=dblAccuracyOut, Status:=lngStatus)
    ' USER DISPLAY
    ' Release objects
    Dim i As Integer
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objModel = Nothing
    Set objProfile = Nothing
End Sub