Solid Edge Part Type Library
GetPhysicalProperties Method
Returns the status of the physical properties of the model. The physical properties can be non-existent, out-of-date, or up-to-date.
Returns the density used when calculating the physical properties.
Returns the accuracy used when computing the physical properties.
Returns the volume of the model.
Returns the surface area of the model.
Returns the mass of the model.
Returns three values that specify the x, y, and z coordinates of the center of gravity of the model.
Returns three values that specify the x, y, and z coordinates of the center of volume of the model.
Returns six values that specify the Ixx, Iyy, Izz, Ixy, Ixz, and Iyz components of the global moments of inertia.
Returns three values that specify the Ixx, Iyy, and Izz components of the principle moments of inertia.
Returns nine values that specify the orientation of the principle axes.
Returns three values that specify the radii of gyration.
Returns the actual accuracy achieved when calculating the physical properties. The accuracy parameter specifies the maximum accuracy, but depending on the geometry of the model, the physical properties can be calculated more accurately.
Description
Returns the current physical properties of the referenced object.
Syntax
Visual Basic
Public Sub GetPhysicalProperties( _
   ByRef Status As Integer, _
   ByRef Density As Double, _
   ByRef Accuracy As Double, _
   ByRef Volume As Double, _
   ByRef Area As Double, _
   ByRef Mass As Double, _
   ByRef CenterOfGravity() As Double, _
   ByRef CenterOfVolume() As Double, _
   ByRef GlobalMomentsOfInteria() As Double, _
   ByRef PrincipalMomentsOfInteria() As Double, _
   ByRef PrincipalAxes() As Double, _
   ByRef RadiiOfGyration() As Double, _
   ByRef RelativeAccuracyAchieved As Double _
) 
Parameters
Status
Returns the status of the physical properties of the model. The physical properties can be non-existent, out-of-date, or up-to-date.
Density
Returns the density used when calculating the physical properties.
Accuracy
Returns the accuracy used when computing the physical properties.
Volume
Returns the volume of the model.
Area
Returns the surface area of the model.
Mass
Returns the mass of the model.
CenterOfGravity
Returns three values that specify the x, y, and z coordinates of the center of gravity of the model.
CenterOfVolume
Returns three values that specify the x, y, and z coordinates of the center of volume of the model.
GlobalMomentsOfInteria
Returns six values that specify the Ixx, Iyy, Izz, Ixy, Ixz, and Iyz components of the global moments of inertia.
PrincipalMomentsOfInteria
Returns three values that specify the Ixx, Iyy, and Izz components of the principle moments of inertia.
PrincipalAxes
Returns nine values that specify the orientation of the principle axes.
RadiiOfGyration
Returns three values that specify the radii of gyration.
RelativeAccuracyAchieved
Returns the actual accuracy achieved when calculating the physical properties. The accuracy parameter specifies the maximum accuracy, but depending on the geometry of the model, the physical properties can be calculated more accurately.
Remarks
The properties returned are the current properties stored with the model, which means they can be not computed yet, out-of-date, or up-to-date. To calculate properties for the first time or to update the properties use the ComputePhysicalProperties method. Properties must not be user-overridden. To determine whether physical properties status, use the PhysicalPropertiesStatus property.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objModel As SolidEdgePart.Model
    ' Dim objBottomCap As Face
    ' Dim objEdges As Edges
    ' Dim objEdgeArray(1 To 4) As Edge
    ' Dim objRound As SolidEdge.Round
    Const TESTFILE = "T:\vbtests\testcases\cube.par"
    Const TOLERANCE = 0.0001
    Dim dblDensity As Double
    Dim dblAccuracyIn As Double
    Dim dblAccuracyOut As Double
    Dim dblVolume As Double
    Dim dblArea As Double
    Dim dblMass As Double
    Dim dblCofGravity() As Double
    Dim dblCofVolume() As Double
    Dim dblGlobalMoments() As Double
    Dim dblPrincipalMoments() As Double
    Dim dblPrincipalAxes() As Double
    Dim dblRadiiOfGyration() As Double
    Dim lngStatus As Long
    Dim dblStartRadiusArray(1 To 4) As Double, dblEndRadiusArray(1 To 4) As Double
    Dim i As Integer
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Close the part document
    Call objDoc.Close
    ' Open a Testcase
    Set objDoc = objApp.Documents.Open(Filename:=TESTFILE)
    ' Get the model object in the test case
    Set objModel = objDoc.Models(1)
    '***************
    ' CASE 1 : ' Attempt to get the physical properties on the model. This
    ' will only work if they've been computed previously.So first compute the
    ' physical properties on the base model and then attempt to get the physical properties
    '***************
    ' Compute the physical properties on the model.
    dblDensity = 1
    dblAccuracyIn = 0.0001
    Call objModel.ComputePhysicalProperties( _
         Density:=dblDensity, Accuracy:=dblAccuracyIn, Volume:=dblVolume, _
         Area:=dblArea, Mass:=dblMass, CenterOfGravity:=dblCofGravity, _
         CenterOfVolume:=dblCofVolume, _
         GlobalMomentsOfInteria:=dblGlobalMoments, _
         PrincipalMomentsOfInteria:=dblPrincipalMoments, _
         PrincipalAxes:=dblPrincipalAxes, _
         RadiiOfGyration:=dblRadiiOfGyration, _
         RelativeAccuracyAchieved:=dblAccuracyOut, Status:=lngStatus)
    ' Checking the physical properties of model
    If (dblVolume - 0.001 > TOLERANCE) Or (dblArea - 0.06 > TOLERANCE) Or _
       (dblMass - 0.001 > TOLERANCE) Or (dblAccuracyOut - 0.0001 > TOLERANCE) Then
        MsgBox ("ComputePhysicalProperties method of Model object fails")
    End If

    ' Get the physical properties on the model.
    Call objModel.GetPhysicalProperties( _
         Status:=lngStatus, Density:=dblDensity, _
         Accuracy:=dblAccuracyIn, Volume:=dblVolume, _
         Area:=dblArea, Mass:=dblMass, CenterOfGravity:=dblCofGravity, _
         CenterOfVolume:=dblCofVolume, _
         GlobalMomentsOfInteria:=dblGlobalMoments, _
         PrincipalMomentsOfInteria:=dblPrincipalMoments, _
         PrincipalAxes:=dblPrincipalAxes, _
         RadiiOfGyration:=dblRadiiOfGyration, _
         RelativeAccuracyAchieved:=dblAccuracyOut)
    ' Checking the physical properties of model
    ' lngstatus value should be one. This indicates properties of the model is up to date.
    If Abs(dblVolume - 0.001) > TOLERANCE Or Abs(dblArea - 0.06) > TOLERANCE Or _
       Abs(dblMass - 0.001) > TOLERANCE Or Abs(dblAccuracyOut - 0.0001) > TOLERANCE Or _
       (lngStatus <> 1) Then
        MsgBox ("GetPhysicalProperties method of Model object fails")
    End If
    '****************
    ' CASE 2 : Change the base model. Without compute get the physical
    ' properties on the updated model
    '****************
    objModel.ExtrudedProtrusions(1).Depth = 0.15
    'Get the physical properties on the updated model. _
     Since the updated model has been not computed so _
     GetPhysicalProperties returns the physical properties of the model
    Call objModel.GetPhysicalProperties( _
         Status:=lngStatus, Density:=dblDensity, _
         Accuracy:=dblAccuracyIn, Volume:=dblVolume, _
         Area:=dblArea, Mass:=dblMass, CenterOfGravity:=dblCofGravity, _
         CenterOfVolume:=dblCofVolume, _
         GlobalMomentsOfInteria:=dblGlobalMoments, _
         PrincipalMomentsOfInteria:=dblPrincipalMoments, _
         PrincipalAxes:=dblPrincipalAxes, _
         RadiiOfGyration:=dblRadiiOfGyration, _
         RelativeAccuracyAchieved:=dblAccuracyOut)
    ' lngstatus value should be zero. This indicates properties of the model to be out of date,
    If (lngStatus <> 0) Then
        MsgBox ("GetPhysicalProperties method of Model object fails for out-of-date values")
    End If
    ' Checking the physical properties of model
    If Abs(dblVolume - 0.001) > TOLERANCE Or Abs(dblArea - 0.06) > TOLERANCE Or _
       Abs(dblMass - 0.001) > TOLERANCE Or Abs(dblAccuracyOut - 0.0001) > TOLERANCE Then
        MsgBox ("GetPhysicalProperties method of Model object fails")
    End If

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objModel = Nothing
End Sub
See Also

Model Object  | Model Members

Send comments on this topic.