Imports System.Runtime.InteropServices
Public Class GetSilverFacesOfBody
    Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDoc As SolidEdgePart.PartDocument = Nothing
        Dim objModels As SolidEdgePart.Models = Nothing
        Dim objModel As SolidEdgePart.Model = Nothing
        Dim objType As Type = Nothing
        Dim dSliverTolerance As Double
        Dim NumSliverFaces As Integer
        Dim SliverFaces(1) As Object
        Dim WidthOfSliverFaces(1) As Double
        dSliverTolerance = 0.2
        Try
            ' Create/get the application with specific settings
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            If objApplication Is Nothing Then
                ' Get the type from the Solid Edge ProgID
                objType = Type.GetTypeFromProgID("SolidEdge.Application")
                ' Start Solid Edge
                objApplication = Activator.CreateInstance(objType)
                ' Make Solid Edge visible
                objApplication.Visible = True
            End If
            ' Get document
            objDoc = objApplication.ActiveDocument
            ' get the models collection
            objModels = objDoc.Models()
            objModel = objModels.Item(1)
            Call objModel.GetSliverFacesOfBody(dSliverTolerance, NumSliverFaces, SliverFaces, WidthOfSliverFaces)
        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try
    End Sub
End Class