Solid Edge Part Type Library
ReadOnly Property
Description
Specifies whether or not the referenced document has been opened as read-only.
Property type
Read-write property
Syntax
Visual Basic
Public Property ReadOnly As Boolean
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim bStat As Boolean
    Const TESTFILE = "T:\vbtests\testcases\chead.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening the test case file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' checking whether the document is read-only
    bStat = objDoc.ReadOnly
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
End Sub
See Also

PartDocument Object  | PartDocument Members

Send comments on this topic.