ActiveSketch | Returns the active Sketch object. |
AddInsStorage | Returns an IUnknown pointer to the object that implements the IStorage corresponding to the add-in substorage for the referenced object. |
AdjustableDefinition | Returns the adjustable definition object. |
Application | Returns the active application object. |
AttachedPropertyTables | Returns the AttachedPropertyTables object for the referenced document object. |
AttributeQuery | Returns the AttributeQuery object. |
AutomaticTransitionToSolutionManager | Determines whether a transition will occur to solution manager automatically after a successful edit. |
BendTable | |
BodyCheck | Specifies whether or not the referenced document object contains a valid parasolid body. |
CapturedRelationshipCount | |
ComponentName | |
ComponentSketches | |
Constraints | |
Constructions | Returns the Constructions collection object. |
CoordinateSystems | Represents a collection of CoordinateSystem objects. |
CreatedVersion | Returns the version of Solid Edge that was used to create the referenced document. |
DesignBodyVisible | Specifies whether or not the referenced object is displayed to the screen. |
DesignEdgebarFeatures | This read-only property returns the EdgeBarFeatures collection object (ordered features) for the referenced object. The collection is dynamically updated, based on history changes. |
DimensionStyles | Returns the DimensionStyles collection object for the referenced document. |
Dirty | Specifies whether or not the referenced document has been modified since the last time it was saved. |
DisableMoveToSynchronous | |
DividedParts | Returns the DividedParts collection object for the referenced Part of Sheet Metal document. |
DividePartEvents | Returns the DividePartEvents object for the referenced document object. |
DocumentEvents | Returns the DocumentEvents object for the referenced document object. |
FaceStyles | Returns the FaceStyles collection object for the referenced document. |
FamilyMembers | Returns the FamilyMembers collection object for the referenced document object. |
FamilyOfPartsEvents | This read-only property returns the FamilyOfPartsEvents collection object for the referenced object. |
FamilyOfPartsExEvents | |
FillStyles | Returns the FillStyles collection object for the referenced document. |
FlatPatternEdgebarFeatures | |
FlatPatternModels | Returns flat pattern models collecton |
FullName | Returns the name and path of the referenced object. |
GeometricVersion | Returns a value that is incremented each time the geometry of an associated document is changed. |
HardwareFile | |
HasCapturedRelationships | |
HatchPatternStyles | Returns the HatchPatternStyles collection object for the referenced document. |
HighlightSets | Returns the HighlightSets collection object for the referenced document object. |
HoleDataCollection | Returns the HoleDataCollection object for the referenced document object. |
InPlaceActivated | Specifies whether or not the referenced document is in-place activated. |
InterpartLinks | |
IsAdjustablePart | Returns whether file is adjustable or not. |
IsFeatureLibrary | Specifies whether or not the referenced PartDocument or SheetMetalDocument is a feature library. |
IsGeometricVersionDirty | Retrieves whether the geometric version number of the assembly document is dirty or not. |
IsMultiCADDriven | |
IsTemplate | Specifies whether or not the referenced document is a template. |
LastSavedVersion | Returns the version of Solid Edge that was used the last time the referenced document was saved. |
Layers | Returns the Layers collection object. |
LinearStyles | Returns the LinearStyles collection object for the referenced document. |
LockedSketch | |
ModelingMode | The property transitions the document between Synchronous and Ordered as is done in the UI via Pathfinder or a context menu. |
Models | Returns the Models collection object for the referenced document object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Path | Returns the directory path name of the referenced document. |
PhysicalPropertiesStatus | This read-only property returns the status of the physical properties of the model for the referenced object. |
ProfileSets | Returns the ProfileSets collection object for the referenced document object. |
ProfileUndoSteps | This read-write Long property sets and returns the number of profile undo steps for the referenced document object. |
Properties | For document objects, returns the PropertiesCollection colletion object. For Variables, sets and returns the variable properties. |
PropertyTableDefinitions | Returns the PropertyTableDefinitions object for the referenced document object. |
ReadOnly | Specifies whether or not the referenced document has been opened as read-only. |
RefAxes | Returns the RefAxes collection object for the referenced document object. |
RefPlanes | Returns the RefPlanes collection object for the referenced document object. |
RootStorage | Returns the IUnknown pointer to the object implementing the root storage of the referenced document. |
RoutingSlip | Returns the RoutingSlip object for the referenced document. |
SelectSet | Returns the current selection set for the referenced document. |
Sensors | Returns the Sensors collection object for the referenced document object. |
ShowCurvatureCombs | Toggles the display of curvature combs for the referenced object. |
SimplifiedModels | Returns the Simplified Models collection object for the referenced document object. |
SimplifyEdgebarFeatures | This read-only property returns the EdgeBarFeatures collection object (ordered features) for the referenced object. The collection is dynamically updated, based on history changes. |
Sketches | Returns the Sketches collection object for the referenced document object. |
Status | Returns the status of the specified object. |
StudyOwner | Get Study Owner object from the document. |
SummaryInfo | Returns a SheetSummaryInfo object to provide access to descriptive properties for the referenced document. |
Terminals | |
Type | Specifies the type of the object being referenced. |
UndoSteps | This read-write Long property sets and returns the number of undo steps for the referenced document object. |
UnitsOfMeasure | Returns the UnitsOfMeasure object for the referenced document. |
UserDefinedSets | |
Variables | Returns the Variables collection object for the referenced document. |
ViewStyles | Returns the ViewStyles collection object for the referenced document. |
Windows | Returns the Windows collection object. |