Solid Edge Part Type Library
SaveAs Method
Specifies the name of the saved file. The other optional parameters are not currently supported.
Not currently supported. However, to save a file as a template, you can save it under the template directory.
When saving as PDF, a value of True saves a 3D PDF where a value of False saves a 2D PDF.  This argument is unsupported for other file types.
Not currently supported.
Not currently supported.
Not currently supported.
Not currently supported.
Not currently supported.
Not currently supported.
Description
Saves the referenced document to a new name, directory, or format.
Syntax
Visual Basic
Public Sub SaveAs( _
   ByVal NewName As String, _
   Optional ByVal IsATemplate As Variant, _
   Optional ByVal FileFormat As Variant, _
   Optional ByVal ReadOnlyEnforced As Variant, _
   Optional ByVal ReadOnlyRecommended As Variant, _
   Optional ByVal NewStatus As Variant, _
   Optional ByVal CreateBackup As Variant, _
   Optional ByVal UpdateLinkInContainer As Variant, _
   Optional ByVal UpdateAllLinksInContainer As Variant _
) 
Parameters
NewName
Specifies the name of the saved file. The other optional parameters are not currently supported.
IsATemplate
Not currently supported. However, to save a file as a template, you can save it under the template directory.
FileFormat
When saving as PDF, a value of True saves a 3D PDF where a value of False saves a 2D PDF.  This argument is unsupported for other file types.
ReadOnlyEnforced
Not currently supported.
ReadOnlyRecommended
Not currently supported.
NewStatus
Not currently supported.
CreateBackup
Not currently supported.
UpdateLinkInContainer
Not currently supported.
UpdateAllLinksInContainer
Not currently supported.
Remarks
When used to copy a source document to a new file name, SaveAs assigns property set values to the new document to give the document a unique identity, changes the name of the document, and updates the window titles and most recently used menu items.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objSummaryInfo As SolidEdgeFramework.SummaryInfo
    Dim varSaveDate As String
    Dim sysTime As String
    Const TESTFILE = "T:\vbtests\testcases\chead.par"
    Const SAVEFILE = "T:\vbtests\TestCases\test.par"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening the test case file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' saving the test case file as another file
    Call objDoc.SaveAs(newname:=SAVEFILE)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSummaryInfo = Nothing
End Sub
See Also

PartDocument Object  | PartDocument Members

Send comments on this topic.