Solid Edge Part Type Library
PatternType Property
Collapse All
Expand All
Solid Edge Part Type Library
>
Pattern Object
: PatternType Property
Description
Sets and returns the pattern to apply to the referenced Pattern object.
Property type
Read-only property
Syntax
Visual Basic
Public Property PatternType As
PatternTypeConstants
Remarks
Depending on the setting of this property, other properties are enabled or disabled. For example, the FillBackGround property is enabled for PatternType = 1, 2, or 3, but is disabled for PatternType = 0.
See Also
Pattern Object
|
Pattern Members
Send comments
on this topic.