Solid Edge Part Type Library
Circles2d Property
Description
Returns the Circles2d collection object for the referenced Profile object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Circles2d As Circles2d
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objCircs As SolidEdgeFrameworkSupport.Circles2d
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create Circles collection object
    Set objCircs = objDoc.ProfileSets.Add.Profiles.Add(objDoc.RefPlanes(1)).Circles2d
    'Create a Circle object
    Call objCircs.AddByCenterRadius(x:=0, y:=0, Radius:=0.01)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objCircs = Nothing
End Sub
See Also

Profile Object  | Profile Members

Send comments on this topic.