Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objProfile As SolidEdgePart.Profile
Dim objPlane As SolidEdgePart.RefPlane
Dim x As Double
Dim y As Double
Dim z As Double
Dim sDumpStatus As String ' Used for temporary storage of datadump return string
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' Create a Profile
Set objPlane = objDoc.RefPlanes.AddParallelByDistance(ParentPlane:=objDoc.RefPlanes(1), _
Distance:=0.05, NormalSide:=igRight)
Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objPlane)
' Calling the Convert2DCoordinate method to convert 2d point to 3d Coordinate
Call objProfile.Convert2DCoordinate(x2d:=1, y2d:=1, x3d:=x, y3d:=y, z3d:=z)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objProfile = Nothing
End Sub