Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
Dim start As Double
Dim finish As Double
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Create a Ellipses 2d collection object
Set objEllpArcs = objDoc.ProfileSets.Add.Profiles.Add(objDoc.RefPlanes(1)).EllipticalArcs2d
'Create an Ellipse object
start = 180 * PI / 180
finish = 230 * PI / 180
Call objEllpArcs.AddByCenter(xCenter:=0.2, yCenter:=0.2, xMajorAxis:=0.5, yMajorAxis:=0.12, Ratio:=0.5, _
Orientation:=igGeom2dOrientClockwise, StartAngle:=start, EndAngle:=finish)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objEllpArcs = Nothing
Set objEllpArc = Nothing
End Sub