Specifies the geometric element for which to return curves. GeometricElement can be a Line2d, Arc2d, EllipticalArc2d, Circle2d, Ellipse2d, BsplineCurve2d, RectangularPattern2d, CircularPattern2d, or Image2d object.
Specifies the number of objects in the Curves array.
Specifies the curves.
Description
Returns one or more curves from the curve body for one of the following geometric elements of the profile: Line2d, Arc2d, EllipticalArc2d, Circle2d, Ellipse2d, BSplineCurve2d, RectangularPattern2d, CircularPattern2d, Image2d or TextProfile2d.
Specifies the geometric element for which to return curves. GeometricElement can be a Line2d, Arc2d, EllipticalArc2d, Circle2d, Ellipse2d, BsplineCurve2d, RectangularPattern2d, CircularPattern2d, or Image2d object.
NumberOfCurves
Specifies the number of objects in the Curves array.