Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfile As SolidEdgePart.Profile
    Dim objRelns As SolidEdgeFrameworkSupport.Relations2d
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim lngSize As Long
    Dim lngStatus As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create a Profile object
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
    Set objLines = objProfile.Lines2d
    Call objLines.AddBy2Points(x1:=0, y1:=0, x2:=0.01, y2:=0)
    Call objLines.AddBy2Points(x1:=0.01, y1:=0, x2:=0.01, y2:=0.01)
    Call objLines.AddBy2Points(x1:=0.01, y1:=0.01, x2:=0, y2:=0.01)
    Call objLines.AddBy2Points(x1:=0, y1:=0.01, x2:=0, y2:=0)
    ' Define Relations among the Line objects to make the Profile closed
    Set objRelns = objProfile.Relations2d
    Call objRelns.AddKeypoint(Object1:=objLines(1), Index1:=igLineEnd, Object2:=objLines(2), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(2), Index1:=igLineEnd, Object2:=objLines(3), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(3), Index1:=igLineEnd, Object2:=objLines(4), Index2:=igLineStart)
    Call objRelns.AddKeypoint(Object1:=objLines(4), Index1:=igLineEnd, Object2:=objLines(1), Index2:=igLineStart)
    ' Validate the Profile
    lngStatus = objProfile.End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox ("Profile Invalid")
    End If
    lngSize = objProfile.Size
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfile = Nothing
    Set objRelns = Nothing
    Set objLines = Nothing
End Sub