| Solid Edge Part Type Library : RefPlanes Collection |
AddAngularByAngle | Creates a reference plane at an angle to an existing reference plane or face and through an edge or an intersection of two faces. |
AddBy3Points | Adds a reference plane by 3 points. |
AddNormalToCurve | Adds a reference plane that is normal to a specified curve. |
AddNormalToCurveAtArcLengthRatio | Adds a reference plane normal to a curve at a specified arc length ratio. |
AddNormalToCurveAtDistance | Adds a reference plane that is normal to a specified curve at a specified distance from the curve. |
AddNormalToCurveAtDistanceAlongCurve | Adds a reference plane normal to a curve at a specified distance along the curve. |
AddNormalToCurveAtKeyPoint | Adds a reference plane normal to a curve at a specified keypoint. |
AddParallelByDistance | Creates a RefPlane object that is parallet to another plane. |
AddParallelByTangent | Creates a reference plane that is parallel to another plane and tangent to a face or plane. |
AddTangentToCurvedSurfaceAtKeyPoint | This method adds a reference plane tangent to a curved surface, that is not a cylinder or cone, at a specified key point. |
AddTangentToCylinderOrConeAtAngle | This method adds a reference plane tangent to a cylinder or cone at a specified angle. |
AddTangentToCylinderOrConeAtKeyPoint | This method adds a reference plane tangent to a cylinder or cone at a specified key point. |
Item | The items in a collection. |
Application | Returns the active application object. |
Count | Returns the number of objects in the referenced collection. |
FeatureGroups | |
Parent | Returns the parent object for the referenced object. |