Solid Edge Part Type Library
AddParallelByTangent Method
Specifies the planar element (reference plane or feature face) to which the reference plane is made parallel.
Specifies the Face object that is tangent to the planar element.
A member of the KeyPointExtentConstants constant set that specifies the tangent position.
Specifies the edge of the parent plane on which the reference plane pivots.
Specifies whether the reference plane should be a local or global reference plane. If not specified, the default is to create a local reference plane. When using Solid Edge interactively, local reference planes are created whenever a profile-based feature is created. Local reference planes are never displayed to the user. Global reference planes are created interactively using the reference plane commands on the reference plane toolbar. Global reference planes are displayed and have their display controlled through the use of various display commands.
Description
Creates a reference plane that is parallel to another plane and tangent to a face or plane.
Syntax
Visual Basic
Public Function AddParallelByTangent( _
   ByVal ParentPlane As Object, _
   ByVal TangentFace As Object, _
   ByVal TangentPositionFlag As KeyPointExtentConstants, _
   Optional ByVal Pivot As Variant, _
   Optional ByVal PivotOrigin As Variant, _
   Optional ByVal Local As Variant _
) As RefPlane
Parameters
ParentPlane
Specifies the planar element (reference plane or feature face) to which the reference plane is made parallel.
TangentFace
Specifies the Face object that is tangent to the planar element.
TangentPositionFlag
ValueDescription
igInteriorReverseTangentNormalKey-point Extent - Interior Reverse Tangent Normal
igInteriorTangentNormalKey-point Extent - Interior Tangent Normal
igReverseTangentNormalKey-point Extent - Reverse Tangent Normal
igTangentNormalKey-point Extent - Tangent Normal
A member of the KeyPointExtentConstants constant set that specifies the tangent position.
Pivot
Specifies the edge of the parent plane on which the reference plane pivots.
PivotOrigin
Local
Specifies whether the reference plane should be a local or global reference plane. If not specified, the default is to create a local reference plane. When using Solid Edge interactively, local reference planes are created whenever a profile-based feature is created. Local reference planes are never displayed to the user. Global reference planes are created interactively using the reference plane commands on the reference plane toolbar. Global reference planes are displayed and have their display controlled through the use of various display commands.
Remarks
The parent plane can be another plane or the planar face of a feature.
See Also

RefPlanes Collection  | RefPlanes Members

Send comments on this topic.